cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Nucleo F103 pinout and Reference Manual mismatch for Usart1 RX/TX

LChio
Associate

On Reference Manual RM0008, pag 186, bit 2, Alternate Function I/O Remap, it stats that the only available pairs for Usart 1 RX/TX can be PA9/PA10 or PB6/PB7, but on the pinout image for the same NUCLEO-F103RB the Usart 1 pinout is on PA2/PA3.

Which one of the two is wrong?

3 REPLIES 3

USART2 uses PA2/PA3

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Imen.D
ST Employee

Hello,

On the pinout: USART2_TX is on PA2 and USART2_RX is on  PA3.

You can also check the pin definitions in the STM32F103 datasheet.

With Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Imen.D
ST Employee

Hello,

On the pinout: USART2_TX is on PA2 and USART2_RX is on  PA3.

You can also check the pin definitions in the STM32F103 datasheet.

With Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen