2018-07-27 04:42 AM
2018-07-27 05:27 AM
Maybe that was a little to brief....
Please start with the serial display, does that have a chip ? 5450 type?
Do you want to increment/decrement a displayed timer ?
Do you need 1mS and 1uSec timers?
Do you want to diplay time ?
2018-07-27 06:34 AM
Thanks for the answer...
the serial display is an old ucn5833a.
I want to increase or decrease time, I need precise timer.
If I have a 1us timer I easily transcode it into a 1ms timer, I think ...
While working only 0.1s.
To view final time or send by uart, here yes with the precision of 1ms, of type xx.xx.xx.xxx
Thank you one more time
2018-07-27 08:07 AM
2018-07-27 08:49 AM
"I need a Ticker of 0.01ms or 0.001ms"
if you meant that you wanted to have interrupts at 10us or 1us, you just need ST to make a MCU that runs at 100 or 1000x of their current offerings.
if you meant that you wanted to have a timer with 10us or 1us resolution, plenty of easy solutions.