cancel
Showing results for 
Search instead for 
Did you mean: 

What should I do with the 3 ADC input pins of the LIS3DH if not used?

Nathalie MAGNIEZ
Associate II
Posted on September 07, 2013 at 17:34

What should I do with the 3 ADC input pins of the LIS3DH if not used?

#lis3dh #motion-sensor #accelerometer #accelerometer
1 REPLY 1
Thiago REIS
Associate II
Posted on September 09, 2013 at 18:26

Hello Naue,

These 3 ADC input pins if not used can be tied to Vdd, or GND, or left floating. From a the power consumption point of view, it is recommended to tie them to either Vdd or GND.

For more details, please check the attached detail sheet and visit

http://www.st.com/mems

Thank you,

Thiago Reis

From: naue

Posted: Saturday, September 07, 2013 5:34 PM

Subject: What should I do with the 3 ADC input pins of the LIS3DH if not used?

________________

Attachments :

LIS3DH.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzKg&d=%2Fa%2F0X0000000bJz%2FtH2q3.U0FmH_73bL0I2AeRlXVRf3wwti0hGbxD3QXiU&asPdf=false