cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L1 up to 512KB Flash

Amel NASRI
ST Employee
Posted on March 05, 2014 at 16:53

STMicroelectronics

 has extended its 

STM32 L1 series

 of ultra-low-power ARM

Cortex

-M3 32-bit microcontrollers with new 512KB flash devices.

0690X00000602rQQAQ.jpg

Key features of the L1 series include

:
  • High-performance ARM Cortex-M3 32-bit core: up to 33 DMIPS operating at 32MHz;
  • Pin-to-pin and software compatibility with all previous STM32 L1 devices;
  • Run-mode dynamic power consumption 257�A/MHz at 32MHz down to 177�A/MHz @ 4MHz
  • Two ultra-low-power modes: down to 435nA with SRAM retention;
  • True embedded EEPROM;
  • Dual-bank flash allowing fast and fail-safe firmware updates and rollback, thanks to the RWW (Read While-Write) capabilities.

The 

STM32 L1 512KB

 is supported by an STM32 Nucleo extension board with mbed

-enabled

.

STM32L1 Series

http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1295

STM32L1

http://www.st.com/web/en/news/n3527

#stm32l1

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

0 REPLIES 0