cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Nucleo boards available for STM32F3 & STM32F0

Amel NASRI
ST Employee
Posted on June 24, 2014 at 18:17

New Easy-to-Use STM32 Tools Add Support for Mixed-Signal and Entry-Level Microcontrollers

 

 

http://www.st.com/web/en/catalog/tools/FM116/SC959/SS1532/LN1847

 development boards are now available for the STM32F3 (

http://www.st.com/web/en/catalog/tools/FM116/SC959/SS1532/LN1847/PF259999

) and STM32F0 lines (

http://www.st.com/web/en/catalog/tools/FM116/SC959/SS1532/LN1847/PF260003

).

The Arduino™ connectivity support and ST Morpho headers make it easy to expand the functionality of the STM32 Nucleo open development platform with a wide choice of specialized shields.

STM32Nucleo boards provide access to all device I/Os and integrate an ST-Link debugger/programmer, saving the need for a separate debug probe.

Also, the STM32Nucleo boards are mbedTM-enabled, so they can be directly connected and run through the online development environment at mbed.org.

The STM32Nucleo boards are available immediately, priced from $10.32.

For further information on STM32Nucleo boards, please visit

http://www.st.com/stm32nucleo

.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

0 REPLIES 0