2008-07-01 09:07 AM
2011-05-17 12:50 AM
If you believe that the rising edge is the problem, I have also tried with the falling edge but without success.
2011-05-17 12:50 AM
Hi fellas,
I have been pulling my hair off during the past two weeks trying to track down the reason(s) behind the following problem. I successfully made the external interrupt 5 work by: 1 - Setting the GPIO3 pin 5 (GPIO3 is enabled in startup file) GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.GPIO_Direction = GPIO_PinInput; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5; GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull ; GPIO_InitStructure.GPIO_IPConnected = GPIO_IPConnected_Disable; //GPIOIN[3] bit 5 set to 0 GPIO_InitStructure.GPIO_Alternate = GPIO_InputAlt1; // does not really matter since pin 5 runs in its default input function GPIO_Init (GPIO3, &GPIO_InitStructure); 2- SCU set up // Connect Pin P3.5 to VIC1.11 chanel SCU->WKUPSEL &= ~0x0005; SCU->WKUPSEL |= 0x0005; 3- VIC 1 set up //VIC1.10 is for external interrupts with button 3 VIC1->VAiR[10] = (unsigned int)&Button_IRQ_Handler; /* Setup external interrupt 5 Hndl addr */ VIC1->INTECR &= 0x0400; // First diasble channel 10 for VIC 1 , to avoid spurious interrupts, as recommended in the reference manual VIC1->VCiR[10] &= 0xFFC0; VIC1->VCiR[10] |= 0x002A; // enable interupt with vector 10 4- WIU set up WIU->TR &= 0x00000000; WIU->TR |= 0x00000040;// Rising edge for external interrupt 5 WIU->PR |= 0xFFFFFFFC; //Clear pendind interupt WIU->CTRL &= 0x00; WIU->CTRL |= 0x02; //Global WIU intr enable WIU->MR &= 0x00000000; WIU->MR |= 0x00000020; //Accept external interupt 5 VIC1->INTER |= 0x0400; // Then Enable channel 10 for VIC 1 5- for the sake of completeness Button_ISR short numberofPushes = 0; __irq void Button_IRQ_Handler (void){ numberofPushes = numberofPushes+1; HW_LED_ioctl(0x20);// simply toggles the LED 0 WIU->PR |= 0xFFFFFFFC; //Clear pending interupt VIC1->VAR = 0; // Clear interupt in VIC1 VIC0->VAR = 0; // Clear interupt in VIC0 } I use Keil µvision V3.53, with Keil MCBSTR9 version 4 (based on STR912FW44) Everything works fine EXCEPT that the ISR gets sometimes executed 2 or 3 times while the button was pushed only once. I was certain of that after I used a memory watch on the variable numberofPushes. Besides, The interrupt is acknowledged in the ISR, and in debug mode I can clearly see that there is no pending interrupt in the VICs registers (in simulated peripherals). Can anyone tell me what's going on here. :-[2011-05-17 12:50 AM
If you are using a mechanical pushbutton switch, how do you debounce it? Switches typically cause several make-break connections as they are closed or released. It sounds like your software is working properly.
2011-05-17 12:50 AM
Thanks for the hint 😉 I am indeed using a mechanical switch.
Any ideas of how to make the ISR REALLY execute once when the button is pushed down?2011-05-17 12:50 AM
Hi, correct me if I'm wrong, but after looking at that posted code, I notice that the rising/falling edge bit is actually set for interrupt 6, not 5. Could this be causing some of your issues?
Posted: 4- WIU set up WIU->TR &= 0x00000000; WIU->TR |= 0x00000040;// Rising edge for external interrupt 5 Should be: 4- WIU set up WIU->TR &= 0x00000000; WIU->TR |= 0x00000020;// Rising edge for external interrupt 52011-05-17 12:50 AM
You could start a timer once you see the first interrupt. That timer disables the button interrupt, and reads the switch after 50ms, re-enabling that interrupt after its done.