cancel
Showing results for 
Search instead for 
Did you mean: 

Reset STR9

dibacco1
Associate II
Posted on March 21, 2008 at 14:08

Reset STR9

2 REPLIES 2
dibacco1
Associate II
Posted on May 17, 2011 at 09:50

I developed a network bootloader using uIP. The bootloader resides in Bank 1, it starts then if it finds a valid application in BB0 runs it.

I need to be able to restart the STR9 from within the application in BB0. Is there any reset instruction?

kais
Associate II
Posted on May 17, 2011 at 09:50

Dear dibacco,

There is no reset instruction, but you can make a Watchdog end of count

Condition (WDG Reset) which is a system reset.

By the way, there is an IAP over Ethernet “AN2675�? already available through this link:

http://www.st.com/mcu/familiesdocs-101.html

Kind regards,

Eris.