cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F207VC DFU

firatparlak
Associate II
Posted on July 16, 2013 at 14:53

Hello,

I'm trying to upgrade my device firmware with the DFU demo for STM32F2xx. I adapted the code from STM32_USB-HostDevice_Lib_V2.1.0\Project\USB_Device_Examples\DFU\MDK-ARM to my project. When the program runs, the DfuSe Demonstration sees ''STM Device in DFU Mode'' in the available DFU devices list. Then I choose a different firmware for my device (which I had tested before) and click upload. But, the DfuSe Demonstration gives the error code of ''... has stopped working.'' 1) I executes the device with the DFU driver code(as in the demo code) 2) Choose a different example.dfu firmware file. 3) Click the DFU button which I'm using in the DFU firmware for entering the mode.

/* Check if the Key push-button on STM32-EVAL Board is pressed */
if(GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_4) == 0x00) //if (STM_EVAL_PBGetState(Button_KEY) != 0x00)
{ /* Test if user code is programmed starting from address 0x800C000 */
if(((*(__IO uint32_t*)APP_DEFAULT_ADD) & 0x2FFE0000 ) == 0x20000000)
{ /* Jump to user application */
JumpAddress = *(__IO uint32_t*) (APP_DEFAULT_ADD + 4);
Jump_To_Application = (pFunction) JumpAddress;
/* Initialize user application's Stack Pointer */
__set_MSP(*(__IO uint32_t*) APP_DEFAULT_ADD);
Jump_To_Application();
}
} /* Otherwise enters DFU mode to allow user to program his application */

4) Finally, click the upload button in the DfuSe Demonstration program. After all, the error code is shown on the display. Looking forward to hear you. #stm32f207 #dfuse-demo #dfu
0 REPLIES 0