cancel
Showing results for 
Search instead for 
Did you mean: 

Self-test LSM330DLC

m2
Associate
Posted on February 07, 2014 at 09:25

Hello,

For a project we are using the LSM330DLC 3D accelerometer and 3D gyroscope module. Chapter 4.1. of the datasheet (Doc ID 022162 Rev 2) mentions self-test functionality, which can be enabled by setting the self-test bit. However none of the registers mentioned in Chapter 8 have a reference to this self-test bit. Could you please indicate in which register this self-test bit is located.

#lsm330dlc-self-test
3 REPLIES 3
dgperkins
Associate
Posted on March 20, 2014 at 11:44

We are also using the LSM330DLC, and would very much like to know whether the chip has a self test mode and how to activate it if so.

William Warke
Associate
Posted on February 24, 2017 at 18:42

Same issue, 3 years later. Any progress on this, or is the self-test feature nonexistent?

Miroslav BATEK
ST Employee

Self test procedure is not available for this product.

Chapter 4.1.1 in datasheet should be removed.