cancel
Showing results for 
Search instead for 
Did you mean: 

External RAM SPC564A example project?

stmicro239955_st
Associate II
Posted on August 04, 2014 at 17:22

Are there any example projects for the SPC564A on the SPC56xxMB EVAL board that show how to use external RAM?

If not complete projects, any code snippets or even hints or advice?

Thanks

Kevin
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee
Posted on August 08, 2014 at 17:13

Hello Kevin ,

On the application wizard , there are 5 test applications :

SPC564Axx OS-Less CAN Test Application

SPC564Axx OS-Less DSPI Example Application

SPC564Axx OS-Less eQADC Example Application

SPC564Axx OS-Less ICU-PWM Test Application

SPC564Axx OS-Less Test Application

I am checking with experts about your requests.

Best regards

View solution in original post

1 REPLY 1
Erwan YVIN
ST Employee
Posted on August 08, 2014 at 17:13

Hello Kevin ,

On the application wizard , there are 5 test applications :

SPC564Axx OS-Less CAN Test Application

SPC564Axx OS-Less DSPI Example Application

SPC564Axx OS-Less eQADC Example Application

SPC564Axx OS-Less ICU-PWM Test Application

SPC564Axx OS-Less Test Application

I am checking with experts about your requests.

Best regards