cancel
Showing results for 
Search instead for 
Did you mean: 

problem with jtag tck pin

m2399
Associate II
Posted on June 01, 2013 at 08:55

hi

I have a problem

with jtag tck pin on my board.

When

I touch

it with

my

finger

  the st-link

Works properly

& connect to stm32f417 but if  i remove my finger from this pin the st-link not connect to my mcu.i pull-down tck pin with 10k to gnd.

Also, when

i connect my board's gnd to pc case

this

problem

can be

solved

.

What is

the problem?why tck pin is sensitive to the touch of my finger

???
2 REPLIES 2
Posted on June 01, 2013 at 13:39

Sounds like some supply connectivity issues, perhaps a schematic and diagram of the connections made would be illustrative.

How is the board powered? How are grounds on the ST-Link connected to your board.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
m2399
Associate II
Posted on June 02, 2013 at 06:45

i convert (2*10 )jtag connector to  header (1*7)  & only use

NRST

TDI

TDO

TCK

TMS

GND

VDD

on my board.also don't use JTAG TRST & pull-up it on my board