cancel
Showing results for 
Search instead for 
Did you mean: 

unable to use SPI interface

bnp979
Associate III
Posted on June 07, 2013 at 08:41

I am trying to access the LSM330DLC devie using the SPI interface without luck. I have religiously tried to follow instructions in the part data sheet to read the WHO_AMI_G register but the there is no output on the SDO pin of the part when I perform a read over the SPI port. Here is how I have setup the part:

* running the SPI clock at 3 Mhz

* CS_G set low and CS_A set high

Is there anything obvious I am missing?

Also, I am trying to figure out the location of the source code for  iNEMO

LI3 engine LITE. The online page for the resource on the STM website has a PDF for no source code.

Can somebody point me to where I can find the code?

Thanks in advance!
0 REPLIES 0