cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F205RBT6 dma queries

aamirali641989
Associate II
Posted on June 12, 2014 at 13:46

1. On page 32 of AN4031 by ST, it says that peripheral should be enable only after DMA stream enabled.

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/application_note/DM00046011.pdf

I have multiple tx & rx on SPI. Like send 2 bytes & then receive 2 byes. Then send 3 bytes & rx 3 bytes & this process has 30 such tx & rx.

Does that mean everytime after each tx/ex I disable SPI & reconfigure DMA ( as no of bytes vary) & reenable SPI again?

Is it suitable for low power application to enable/reenable peripherals in consecutive transactions or do it without DMA then semd CPU to sleep mode? 

0 REPLIES 0