cancel
Showing results for 
Search instead for 
Did you mean: 

No target connected on STM32F373CB

projnikdroid
Associate II
Posted on December 24, 2013 at 08:19

As m a newbie to STM32 need help on following:

I am using ST-Link from STM32F0 discovery board (jumpers removed as provided in PDF), for connection with STM32F373xx .

Connections:

SWD(on F0)                     PINS ON MCU(STM32F373CB)

1                                           Connected to VDD_1(pin no 48)

2                                           SWCLK (pin no 37)

3                                           GND(pin no 47)

4                                            SWDIO (pin no 34)

5                                            NRST

while VDD_1, VDD_2 and VDDA are connected to 3V of F0 BOARD.

It shows ''No Target Connected''.(Settings of SW in the IDE are done and selected STLINK Debugger)

#no-target-coonected-stm32f373xx
0 REPLIES 0