2014-09-01 05:50 PM
I am using STM32F2xx and connect it with FT232 chip using UART interface
http://www.ftdichip.com/Products/ICs/FT232R.htmand then I connect FT232 chip to my Windows PC, I wrote an application in my PC using .Net to read and write data to the chip. The PC side is connected to FT232 chip using Virtual Com Port.I found out that, I could not achieve serial speed higher than 1Mbit/s, which is far lower than advertised by them 12Mbit/s, (the common high speed spec),I tried to set different baudrate in STM32, if I would set higher than 1250000 baudrate, I would start to get error in the UART bus, May I know how can I achieve high serial communication speed?2014-09-01 06:29 PM
You'd need to pick rates that will divide cleanly into 1/16th of the APB clock your USART resides on.
Especially with high rates you're going to have to pay particular attention to the error in the baud rates selections (desired vs actual). Async serial is not particularly recommended for rates >921600 baud2014-09-01 06:44 PM
Thank you for your reply!
May i know how can I get the APB clock from my device? I am currently using STM32F205RE?If baudrate > 921600 baud is not recommended, how can I achieve the high speed data transmission?2014-09-01 07:47 PM
Well what are you setting the PLL and bus dividers too? system_stm32f2xx.c
RCC_GetClockFreqs() ? Something using Bulk Mode, and large blocks of data...2014-09-01 07:53 PM
2014-09-01 08:09 PM
I have attached a screenshot of my PLL settings in system_stm32f2xx.c
I have tried to send large block of data at once, but it doesnt seems to help increase the speed, currently I am sending 18 bytes per send, How can I enable bulk mode transfer in STM32?? any resources?? Thanks for your great help! ________________ Attachments : stm32.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I10L&d=%2Fa%2F0X0000000biG%2Fk4x1QdvudqUAckoNlAj.Z_twLg5CNUPeD8lxBM5BRfQ&asPdf=false2014-09-03 06:38 AM
Hi
''How can I enable bulk mode transfer in STM32?? any resources??'' Unless I have not understood correctly - you cannot! I think 'bulk mode' is something that USB implements. In your set up, you are only use the USART. The FTDI chip implements the USB in your system, it is therefore out of your hands. I have not looked at the FTDI chip for ages but you might be able to change some of it's configuration through some of the pins but I do not know for sure. What Clive1 is trying to tell you is to increase the baud rate of the USART to the maximum the STM32 can achieve and the FTDI device will accept.