cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F07x, STM32F08x and STM32F09x are dummy products???

Osto
Senior
Posted on November 06, 2015 at 13:19

Hi,

I have a new project which would run on STM32F051K8T but need more than 64K flash.

I saw the STM32F0[789]x has more flash but nobody sell them!?

Mouser, Digikey,.... have not one of this series.

Do somebody sell them at all? Or are they only on paper?

Regards,

Osto
2 REPLIES 2
Uwe Bonnes
Principal II
Posted on November 06, 2015 at 13:44

Try http://www.findchips.com

F072 seems to be available at several places, e.g. Farnell.

Nesrine M_O
Lead II
Posted on November 06, 2015 at 14:32

Hi Osto,

Look to the ST website to have an idea about product distributor availability, for example

http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1574/LN1826/PF261320#

 

-Syrine-