cancel
Showing results for 
Search instead for 
Did you mean: 

is there an ST-LINK V2 with the V2-A version firmware?

dirkvermaak
Associate II
Posted on June 22, 2016 at 11:18

Hi,

Does anyone know if there is an ST-Link (the actual small white unit) that runs the V2-A firmware that allows the  Mass storage option? 

I have an STM32F407G-DISC1 with this feature (with ST-LINK/V2-A only) and it's great. However I have a custom board coming back and now need to use the external unit.

It is possible to upgrade the firmware in the ST-Link?

Many Thanks,

Dirk Vermaak

#st-link #stm32f4
1 REPLY 1