2013-07-30 01:23 AM
I connect USART1 or 2 via adapter Usb2Com but the terminal displays strange symbols....
&sharpinclude ''stm32f0xx.h''&sharpinclude ''stm32f0xx_rcc.h''&sharpinclude ''stm32f0xx_gpio.h''&sharpinclude ''stm32f0xx_usart.h'' int main(void){ USART_InitTypeDef USART_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2,ENABLE); GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_1); GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_1); //Configure USART2 pins: Tx and Rx ---------------------------- GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStructure); USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART2, &USART_InitStructure); USART_Cmd(USART2,ENABLE); while(1) { while (USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); // Wait for Empty USART_SendData(USART2, '3'); // Send 'I' } return 0; } #stm32 #discovery2013-07-30 03:03 AM
First hint: baudRate, second hint - encoding.
What bothers me is this comment: USART_SendData(USART2, '3'); // Send 'I' <---???? Care to explain?2013-07-30 03:31 AM
Yes, there is not erased the comment, I tried to bring other characters...
2013-07-30 05:44 AM
So is receiving part of terminal set properly? You are trying to send '3' ASCII (hopefully) and you should receive anything like 51 0x33 or something - really dependent how you set your receiving terminal.
2013-07-30 08:20 AM