cancel
Showing results for 
Search instead for 
Did you mean: 

DCMI Not generating interrupt ??

zeros_and_ones1991
Associate III
Posted on July 20, 2014 at 20:23

Hullo guys , I 'm writing my own Library for OV7670 Cam , using DCMI , I could talk to the cam properly through I2C , n now the probelm is that im trying to generate the LINE (HSYNC) interrupt as part of the testing , ( without using the DAM yet) , n the interrupt is never generated , I tried to put the HSYNC pin of the cam on scope , and it is working as it should .

Here is my IO ,  DCMI and NVIC Configurations

//

//

//D0->PA9

//D1->PA10

//D2->PC8

//D3->PC9

//D4->PC11

//D5->PB6

//D6->PB8

//D7->PB9

//HSYNC->PA4

//VSYNC->PB7

//PIXEL_CLK->PA6

//XCLK->PA8(MCO1)

DCMI_InitTypeDef DCMI_Struct;

NVIC_InitTypeDef NVIC_DCMI ;

GPIO_InitTypeDef GPIO;

    // Enable IO clock

    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA | RCC_AHB1Periph_GPIOB | RCC_AHB1Periph_GPIOC, ENABLE);

     //IO initialize

    // GPIOA (4,6,9,10)

    GPIO.GPIO_Mode=GPIO_Mode_AF;

    GPIO.GPIO_OType=GPIO_OType_PP;

    GPIO.GPIO_Speed=GPIO_Speed_100MHz;

    GPIO.GPIO_PuPd=GPIO_PuPd_NOPULL;

    GPIO.GPIO_Pin=GPIO_Pin_4 | GPIO_Pin_6 | GPIO_Pin_9 | GPIO_Pin_10;

    GPIO_PinAFConfig(GPIOD, GPIO_PinSource4, GPIO_AF_DCMI);

  GPIO_PinAFConfig(GPIOD, GPIO_PinSource6, GPIO_AF_DCMI);

  GPIO_PinAFConfig(GPIOD, GPIO_PinSource9, GPIO_AF_DCMI);

  GPIO_PinAFConfig(GPIOD, GPIO_PinSource10, GPIO_AF_DCMI);

    GPIO_Init(GPIOA, &GPIO);

    //

    //  GPIOB (6,7,8,9)

    GPIO.GPIO_Pin=GPIO_Pin_6 | GPIO_Pin_7 | GPIO_Pin_8 | GPIO_Pin_9 ;

    GPIO_PinAFConfig(GPIOD, GPIO_PinSource6, GPIO_AF_DCMI);

  GPIO_PinAFConfig(GPIOD, GPIO_PinSource7, GPIO_AF_DCMI);

  GPIO_PinAFConfig(GPIOD, GPIO_PinSource8, GPIO_AF_DCMI);

  GPIO_PinAFConfig(GPIOD, GPIO_PinSource9, GPIO_AF_DCMI);

    GPIO_Init(GPIOB, &GPIO);

    //

    //

    // GPIOC (8,9,11)

    GPIO.GPIO_Pin=GPIO_Pin_8 | GPIO_Pin_9 |GPIO_Pin_11;

    GPIO_PinAFConfig(GPIOD, GPIO_PinSource6, GPIO_AF_DCMI);

  GPIO_PinAFConfig(GPIOD, GPIO_PinSource7, GPIO_AF_DCMI);

  GPIO_PinAFConfig(GPIOD, GPIO_PinSource8, GPIO_AF_DCMI);

    GPIO_Init(GPIOC, &GPIO);

    //

// Configure the DCMI

    // Enable the Clck of the DCMI module

    RCC_AHB2PeriphClockCmd (RCC_AHB2Periph_DCMI , ENABLE);

    // Reset the DCMI Registers

    RCC_AHB2PeriphResetCmd(RCC_AHB2Periph_DCMI, ENABLE);

   RCC_AHB2PeriphResetCmd(RCC_AHB2Periph_DCMI, DISABLE);

    //

    // Configure the DCMI

    DCMI_Struct.DCMI_CaptureMode=DCMI_CaptureMode_SnapShot;

    DCMI_Struct.DCMI_CaptureRate=DCMI_CaptureRate_All_Frame;

    DCMI_Struct.DCMI_ExtendedDataMode=DCMI_ExtendedDataMode_8b;

    DCMI_Struct.DCMI_HSPolarity=DCMI_HSPolarity_Low;

    DCMI_Struct.DCMI_PCKPolarity=DCMI_PCKPolarity_Rising;

    DCMI_Struct.DCMI_VSPolarity=DCMI_VSPolarity_High ;

    DCMI_Struct.DCMI_SynchroMode=DCMI_SynchroMode_Hardware;

    DCMI_Init(&DCMI_Struct);

    //

    // Enable the NVIC for the DCMI

    NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0);

    NVIC_DCMI.NVIC_IRQChannel=DCMI_IRQn;

    NVIC_DCMI.NVIC_IRQChannelCmd=ENABLE;

    NVIC_DCMI.NVIC_IRQChannelPreemptionPriority=1;

    NVIC_DCMI.NVIC_IRQChannelSubPriority=1;

    NVIC_Init(&NVIC_DCMI);

    //

    // Enable the DCMI Interrupts

    DCMI_ITConfig(DCMI_IT_LINE  , ENABLE); // LINE

    //

    // Enable the Capture mode

    DCMI_CaptureCmd(ENABLE);

    DCMI_Cmd(ENABLE);

//

//

I never get into the Interrupt handler of the DCMI ....... Any ideas ?
2 REPLIES 2
Posted on July 21, 2014 at 03:13

So NOT GPIOD for all the other pins in GPIO_PinAFConfig() !!!

// GPIOA (4,6,9,10)
GPIO.GPIO_Mode=GPIO_Mode_AF;
GPIO.GPIO_OType=GPIO_OType_PP;
GPIO.GPIO_Speed=GPIO_Speed_100MHz;
GPIO.GPIO_PuPd=GPIO_PuPd_NOPULL;
GPIO.GPIO_Pin=GPIO_Pin_4 | GPIO_Pin_6 | GPIO_Pin_9 | GPIO_Pin_10;
GPIO_PinAFConfig(GPIOD, GPIO_PinSource4, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource6, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource9, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource10, GPIO_AF_DCMI);
GPIO_Init(GPIOA, &GPIO);
//
// GPIOB (6,7,8,9)
GPIO.GPIO_Pin=GPIO_Pin_6 | GPIO_Pin_7 | GPIO_Pin_8 | GPIO_Pin_9 ;
GPIO_PinAFConfig(GPIOD, GPIO_PinSource6, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource7, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource8, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource9, GPIO_AF_DCMI);
GPIO_Init(GPIOB, &GPIO);
//
//
// GPIOC (8,9,11)
GPIO.GPIO_Pin=GPIO_Pin_8 | GPIO_Pin_9 |GPIO_Pin_11;
GPIO_PinAFConfig(GPIOD, GPIO_PinSource6, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource7, GPIO_AF_DCMI);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource8, GPIO_AF_DCMI);
GPIO_Init(GPIOC, &GPIO);
//

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
zeros_and_ones1991
Associate III
Posted on July 21, 2014 at 04:11

OMG , thx a lot clive , i was copying the Pin config from another file (saving few seconds lol) , n it turned out to wast few hours not to notice that . Its working ok now .

THX again man .