2014-05-15 09:09 AM
Hi
I just can't understand this... So, I'm communicating with PC's terminal program via USART2 on my STM32F10. Communication is running smoothly both ways, but I have a problem when I want my embedded system to respond appropriately to PC's commands. Basically, when ''I'' receive 9 characters, I read the first character and optionally what's behind, but mostly just 1st character matters. So, if I send for example 9 x m (RxBuffer = ''mmmmmmmmm'') or any combination of 'm' and ''whatever follows'', it seems to work fine, and the LED goes off. Similarly with 'c' (LED goes ON). But, if I send i.e. ''t01100100'' or ''ttttttttt'', switch interprets it as 'm'. o_O Well, screenshot says it all. Thanks for taking time 🙂2014-05-15 09:18 AM
The break is on the for, not the case
You will need a break on the case to stop it falling through to the next one, which is default switch/case behaviour defined by the language.2014-05-15 09:25 AM
Thanks for noticing, howerer it doesn't solve it. The behaviour is completely the same.
2014-05-15 09:43 AM
Post the code, I can't edit text in graphical format....
2014-05-16 12:59 AM
void react_on_cmd(void) //reaction to receiving a command through USART
{ uint8_t i; switch(RxBuffer[0]) { case 'c': { mode = calibration; break; } case 't': { for (i = 1; i == sizeof(active_sensor_table); i++){ active_sensor_table[i] = RxBuffer[i]; } break; } case 'm': { mode = measurement; break; } //case 's': start measurement... //RxCounter = 0; default: { strcpy(TxBuffer, ''\nCommunication error''); //send RST indicator to PC TxCounter = 0; USART_ITConfig(USART2 , USART_IT_TXE , ENABLE); } } if(mode) STM32vldiscovery_LEDOn(LED3); else STM32vldiscovery_LEDOff(LED3); } Is this sufficient or you need other parts of program?2014-05-16 01:37 AM
Hi !
One thing first, don't put braces around case statements, i.e.switch(expression){ case 1: ... break; case 2: ... break; default: ... break;}Second thing, in case't', the for loop will never execute, unless active_sensor_table has only one element. It should be defined as(for i = 1; i < sizeof(active_sensor_table); i++){...}Then if your table contains words, since sizeof(active_sensor_table) will give you the size in bytes, you'll have a runaway pointer for sure...Have a nice day2014-05-16 02:59 AM
Wau, thanks, i think those brackets were the issue (gotta relearn the syntax i guess :))! I also repaired the sizeof() - countof = (sizeof (a)/sizeof(*a)).
Take carevoid react_on_cmd(void) //reaction to receiving a command through USART
{ uint8_t i; switch(RxBuffer[0]) { case 'c': mode = calibration; break; case 't': for (i = 0; i <= (countof(active_sensor_table)-1); i++){ active_sensor_table[i] = RxBuffer[i+1]; } break; case 'm': mode = measurement; break; //case 's': start measurement... //RxCounter = 0; default: strcpy(TxBuffer, ''\nCommunication error''); //send RST indicator to PC TxCounter = 0; USART_ITConfig(USART2 , USART_IT_TXE , ENABLE); } if(mode) STM32vldiscovery_LEDOn(LED3); else STM32vldiscovery_LEDOff(LED3); }2014-05-16 03:31 AM
Wau, thanks, i think those brackets were the issue (gotta relearn the syntax i guess :))!
Actually, the practice of putting case branches into brackets, is perfectly legal and often seen (albeit I strongly dislike it, too). It usually makes no sense - except to create a new context for declaring local variables.
2014-05-16 05:18 AM
Ah, since I have never seen this before, I assumed it was not correct. As you (fm) said, it is only meaningful for handling very local variable (and of course I also (wrongly) assumed that each case had its own context).