2013-08-26 01:45 PM
Hi, I'm trying to run the ''USB Device VCP example'' using the gcc (sourcery-lite) tools. I can build it and it appears to be running (led is blinking and the message ''USB device library started'' comes out the UART; but then I get ''Unknown Device'' on the USB side when I plug it into a PC.
Has anyone built any of the USB device demos with GCC? #usb2013-08-26 01:54 PM
Has anyone built any of the USB device demos with GCC?
Yes, both VCP and MSC. The VCP enumerates in a somewhat squirrely fashion whether GNC/GCC or Keil is used.2013-08-26 02:29 PM
That's good to hear. I must have something screwed up with my translation from the project files used under MDK-ARM (I assume this is Keil) and my makefile with gcc. Didn't look like anything too tricky, but I've yet to get it running, so apparently I'm missing something...
I have the Discovery board mounted on the STF4BB base board so I've got USART6 connected to my PC along with the USB cable for VCOM on the other end. I steer the printf output of the application to that USART, and at startup I see the message ''USB device library started'', and then the LED just keeps blinking, so it appears that all is sane.I updated the system_stm32f4xx.c file to match the board (clock/pll/etc...) and other than that I just use -mcpu=cortex-m4 -mthumb-D USE_STDPERIPH_DRIVER -D STM32F4XX -D USE_USB_OTG_FS to complile each file, then link it. Are there any other mods that need to be made to this for a GCC build? Hey, better yet, is there a makefile out there somewhere that I could just shamelessly steal for this?UPDATE: actually, the above isn't quite true... if I use just ''-D USE_USB_OTG_FS'' the LED does not blink; if i build with -D USE_USB_OTG_HS -D USE_ULPI_PHY then the LED blinks continuously.2013-08-26 05:01 PM
https://docs.google.com/file/d/0B7OY5pub_GfIdnREeExyRWNXbFE/edit?usp=sharing
2013-08-28 06:21 AM
Sorry for the late reply (was out of office yesterday). Thanks much, I'll try this today.
Meanwhile, I noticed quickly that this code is quite different than the code that comes with examples .zip file as supplied by Element14 where I purchased the board-set. Is there a more up-to-date version of that set of examples?2013-08-28 06:35 AM
Is there a more up-to-date version of that set of examples?
I guess that would be something you need to discuss with Element 14, I'm not responsible for their code, or ST's for that matter. I built my code using the most current/appropriate firmware at the time I put it together. You could download ST's from the site here, and then merge/diff to see what changed.
2013-08-28 10:08 AM
Ok, I was able to build and run your source, thanks much.
I added support for USART6 which is the default (jumperable) tied to the DB9 connector of the DMSTF4BB expansion board. One thing I noticed (regardless of whether I use USART2 or USART6), I only see data characters from VCP to USART, but not USART to VCP. Is that expected?BTW, if you want the USART6 change let me know. It uses USART2 by default but -D USE_USART6 makes the change.2013-08-28 11:14 AM
2013-08-29 08:06 AM
Ok, I managed to get bidirectional data working, but I don't quite understand the problem.
Maybe you can shed some light on this...I managed to narrow the problem down (it never ceases to amaze me just how much debugging you can do with a few leds!) to determine that the variable 'APP_Rx_ptr_in' was not being initialized to zero. Looking at the memory map with objdump I saw some very odd entries...out/demo.elf: file format elf32-littlearm
architecture: arm, flags 0x00000112:EXEC_P, HAS_SYMS, D_PAGEDstart address 0x08000188Sections:Idx Name Size VMA LMA File off Algn 0 .isr_vector 00000188 08000000 08000000 00008000 2**0 CONTENTS, ALLOC, LOAD, READONLY, DATA 1 .text 00002410 08000188 08000188 00008188 2**2 CONTENTS, ALLOC, LOAD, READONLY, CODE 2 .data 0000013c 20000000 08002598 00010000 2**2 CONTENTS, ALLOC, LOAD, DATA 3 .bss 00000f94 2000013c 080026d4 0001013c 2**2 ALLOC 4 .bss.cfgidx.8217 00000001 200010d0 08003668 0001013c 2**0 ALLOC 5 .bss.USBD_cfg_status 00000004 200010d4 0800366c 0001013c 2**2 ALLOC 6 .bss.USBD_ep_status 00000004 200010d8 08003670 0001013c 2**2 ALLOC 7 .bss.USBD_default_cfg 00000004 200010dc 08003674 0001013c 2**2 ALLOC 8 .bss.usbd_cdc_AltSet 00000004 200010e0 08003678 0001013c 2**2 ALLOC 9 .bss.USB_Tx_State 00000001 200010e4 0800367c 0001013c 2**0 ALLOC 10 .bss.cdcLen 00000004 200010e8 08003680 0001013c 2**2 ALLOC 11 .bss.APP_Rx_ptr_in 00000004 200010ec 08003684 0001013c 2**2 ALLOC 12 .bss.APP_Rx_ptr_out 00000004 200010f0 08003688 0001013c 2**2 ALLOC 13 .bss.FrameCount 00000004 200010f4 0800368c 0001013c 2**2 ALLOC 14 .bss.APP_Rx_length 00000004 200010f8 08003690 0001013c 2**2 ALLOC 15 ._usrstack 00000100 10000000 10000000 00018000 2**0 ALLOC 16 .comment 00000070 00000000 00000000 0001013c 2**0 CONTENTS, READONLY 17 .ARM.attributes 0000002f 00000000 00000000 000101ac 2**0 CONTENTS, READONLY 18 .debug_aranges 00000978 00000000 00000000 000101e0 2**3 CONTENTS, READONLY, DEBUGGING 19 .debug_info 000139de 00000000 00000000 00010b58 2**0 CONTENTS, READONLY, DEBUGGING 20 .debug_abbrev 00002ffd 00000000 00000000 00024536 2**0 CONTENTS, READONLY, DEBUGGING 21 .debug_line 00008458 00000000 00000000 00027533 2**0 CONTENTS, READONLY, DEBUGGING 22 .debug_frame 000015f0 00000000 00000000 0002f98c 2**2 CONTENTS, READONLY, DEBUGGING 23 .debug_str 0005a77f 00000000 00000000 00030f7c 2**0 CONTENTS, READONLY, DEBUGGING 24 .debug_loc 00005d75 00000000 00000000 0008b6fb 2**0 CONTENTS, READONLY, DEBUGGING 25 .debug_ranges 00000970 00000000 00000000 00091470 2**3 CONTENTS, READONLY, DEBUGGING 26 .debug_macro 0001123d 00000000 00000000 00091de0 2**0 CONTENTS, READONLY, DEBUGGINGNotice all those ''.bss.XXXXX'' sections, one of which is .bss.APP_Rx_ptr_in.
For some reason the linker is putting some variables in their own sections. Unfortunately, they are outside of the areas that are mapped for initialization in startup_stm32f4xx.s. I haven't been able to nail down why that's happening, but I was able to work around this by forcing the initialization of each of these variables at the top of main. After doing that, magically I now have data transfer in both directions.Have you ever seen this behavior before?I'm using gcc version 4.7.3 20130312 on Cygwin.2013-08-29 09:10 AM
The release has an earlier .LD file, you need to add *(.bss.*) into the .bss section
/* This is the uninitialized data section */
.bss :
{
. = ALIGN(4);
/* This is used by the startup in order to initialize the .bss secion */
_sbss = .;
*(.bss)
*(.bss.*)
*(COMMON)
. = ALIGN(4);
/* This is used by the startup in order to initialize the .bss secion */
_ebss = . ;
} >RAM
I use Yagarto for GNU/GCC under Windows.