cancel
Showing results for 
Search instead for 
Did you mean: 

Problem about keil-mdk connect STM32F405,but keil noticed''unknow target connect''

782435875
Associate
Posted on August 22, 2013 at 12:05

I have chose the STM32F405RG and the st-link debugger.

The program is used for STM32F407-DISCOVERY at first.It can work at the STM32F407-DICOVERY,but after I changed the device and other options.

0690X00000602pZQAQ.jpg

0690X00000602pUQAQ.jpg

0690X00000602pfQAA.jpg
2 REPLIES 2
Posted on August 22, 2013 at 13:13

Make sure to use ''SWD'' mode.

See if adapter is visible as ''ST Link (Deprecated)'' if it has older firmware. For problems with software on the board, reset with BOOT0 = High
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
782435875
Associate
Posted on August 23, 2013 at 07:39

I was use the ''JTAG'' mode,and I'm sure that I have connected right in the light of the datasheet.

But both BOOT0 and BOOT1 connect nothing.May it is wrong here?

One more question,when I use I2C,the voltage is up to 5V.

And it have been connected to the pin-29 and pin-30.May I do like this?