cancel
Showing results for 
Search instead for 
Did you mean: 

SDCC 3.5.0 released

Philipp Krause
Senior II
Posted on June 24, 2015 at 15:12

SDCC is a free C compiler targeting 8-bit architectures. This is the second release supporting the STM8, and STM8 users will see a substantial number of improvements compared to the previous 3.4.0. A recent presentation on SDCC can be found at

http://video.fosdem.org/2015/devroom-embedded/8bit_compiler.mp4

Philipp P.S.: See below for the release announcement:

Hello SDCC friends, Today a new release of SDCC was made. We are now at version 3.5.0. You can get it at:

http://sourceforge.net/projects/sdcc/files/

So what's new? * --disable-non-free configure option * Changed default language dialect from --std-sdcc89 to --std-sdcc99 * Reorganized and updated manual * Reduced memory consumption (most noticeable for high --max-allocs-per-node) * Faster compilation for stm8 (most noticeable for high --max-allocs-per-node) * atoll() function for conversion of strings to long long * __z88dk_fastcall and __z88dk_callee calling conventions for more efficient function calls and better compability with z88dk * --lospre-unsafe-read renamed to --allow-unsafe-read And of course numerous feature requests and bug fixes are included as well. Once again I hope you will enjoy using this new release. Maarten Brock SDCC 3.5.0 Release Manager
0 REPLIES 0