2014-04-03 04:08 AM
Hey guys,
I'm trying to calculate a md5 hash on a string I've got and I'm calling the function:HASH_MD5((uint8_t *)buffer, size, Md5output);where size is the size of the buffer. But the Md5output is empty after execution. Is there something I'm missing other than that line? The only other thing I've done is enable the clock:RCC_AHB2PeriphClockCmd(RCC_AHB2Periph_HASH, ENABLE);2014-04-03 04:16 AM
Bit of extra info:
the buffer is defined as a string and contains the text ''042ACE880483B3\r\n03.04.2014 12:12:20\r\n'' The result of the HASH_MD5 is success so not quite sure what is going on. Md5output is defined as uint8_t Md5output[16] and size is an integer 37.2014-04-07 12:55 AM
Has no one had any experience with the hash library?
2014-04-08 03:04 AM
There is an example within the STM32F4 Standard peripheral library (Project\STM32F4xx_StdPeriph_Examples\HASH\HASH_SHA1_MD5). You can try it & check if you still have an issue.
-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2014-04-08 08:03 AM
2014-04-08 08:18 AM
From an F215
---------------------------------------
MD5 Hash Data:
---------------------------------------
02 93 21 E4 4A DD 8C 0D 11 DF 8B DA 66 21 10 7C