cancel
Showing results for 
Search instead for 
Did you mean: 

Hardware NSS management

hilwan
Associate II
Posted on April 17, 2014 at 14:59

Hi all;

I'm trying to connect to F3 Discovery board using SPI in full duplex. One acting as master, the other as a slave.

I have succeed to get them work with no problem if the Software NSS management is configured. But, in the master side, when i use Hardware NSS management, it doesn't work.

In fact, i use both the USB  and SPI protocol. My USB is implemented as HID.

If  SPI_InitStructure.SPI_NSS =SPI_NSS_Hard; my device becomes

unrecognized

.

Do you have an idea about this problem?

Thanks in advance for any help

0 REPLIES 0