cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot change system speed for STM32F746IG

juriedutoit
Associate II
Posted on July 06, 2016 at 08:42

I designed a PCB and I am programming the STM32F746IG via a FT2232D chip.  I have the 4 x JTAG signals connected to the STM32.

I generate code with MXCube, it compiles, but when I run it, Crossworks goes into an enless loop giving me gives me ''Stopped by Vector Catch''.  I have pin pointed it to the function : main.c -> SystemClock_Config(void) -> ''if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)'' -> ''__HAL_RCC_PLL_ENABLE();'' (just after the call to ''WRITE_REG(...)'')

I also used MXCube to generate a Keil MDK V5 project, it compiled, but the same happened in the Keil development environment.

How do one change the clock frequency of the PLL to 216MHz?

Please advise!

Thanks
1 REPLY 1
Posted on July 06, 2016 at 15:29

[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/Cannot%20change%20system%20speed%20for%20STM32F746IG&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000F9A0E3A95BA69146A17C2E80209ADC21&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Java/AllItems.aspx&currentviews=7]cross posted

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..