cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Ethernet Port (TCP Throughput)

whwong84
Associate II
Posted on May 28, 2018 at 12:09

Hi Guys,

I am currently performing the TCP throughput Test by using lwiperf framework as provided. I have performed the test on below Nucleo 144 pins board,

  1. NUCLEO-F207ZG
  2. NUCLEO-F746ZG

Both of the boards are running a modified version from LwIP_HTTP_Server_Netconn_RTOS, where it includes iperf framework.

But the test result seems strange, it shows that the TCP throughput is not dependent on the MCU speed. Both MCU, STM32F2 and STM32F7 gives me similar result. Result as per screenshot attached.

Result for STM32F2

0690X0000060KuHQAU.png

Result for STM32F7

0690X0000060KuIQAU.png

My question, is the throughput (bandwidth) of the Ethernet MAC Controller is not dependent on the speed of the MCU?

0 REPLIES 0