cancel
Showing results for 
Search instead for 
Did you mean: 

STM3240G-EVAL & STM3240G-ETH UDP Serial Loop Back

daniel1
Associate
Posted on October 07, 2013 at 14:35

Good day

I am an Engineering student currently busy with a final project. What the project breaks down to is that I have an application on Windows that sends a UDP packet to a STM3240G-EVAL & STM3240G-ETH. The kits have to be able to read the packet, send packet data over serial / GPIO, loop back on itself then send the data back over UDP. Effectively it loops whatever message it receives from UDP over the serial then back through UDP.  I have to compare the two eval kits against each other that is the reason that both are used.

Now my problem is that I have never worked within the ST environment nor do I know how to do this. I have written the Windows application and I am able to send and receive with it, so that side is not an issue. 

Can someone please assist me with the coding for these kits as it is very urgent!

Many thanks in advance!

Daniel Schoeman

#serial #udp #stm3240g-eval
1 REPLY 1
Posted on October 07, 2013 at 17:54

What's the hourly rate for

http://www.catb.org/esr/faqs/smart-questions.html#urgent

these days?

STM32F4x7_ETH_LwIP_V1.0.0\Project\Standalone\udp_echo_server
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..