cancel
Showing results for 
Search instead for 
Did you mean: 

Illegal address on stm32f3discovery in debug mode

andreaspiezia9
Associate III
Posted on November 06, 2013 at 11:29

Hi all,

I'm starting the debug with Keil uVision V4.72.10.0.

Compile and programming is OK, but when I start the debug session the output window show the next error message:

Internal DLL Error

 

Internal command error

 

*** error 57: illegal address (0x08000000)

I've set the target option as indicated in the 

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00062662.pdf

 on page 28 Fig 32.

Can you help me?

Thanks and regards

 
1 REPLY 1
Posted on November 06, 2013 at 13:30

Have you tried using the Template project? Does that work?

Make sure not to use the ''ST-Link Deprecated'', that the Debug/Setup dialog shows it finds the device, FW version, SWD, etc. Make sure you've loaded current drivers (\Keil\ARM\ST-Link ?)

It might be helpful to provide screen shots of your configurations.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..