cancel
Showing results for 
Search instead for 
Did you mean: 

Feed Two GPIO From Same Timer?

jvavra
Associate III
Posted on September 19, 2014 at 16:25

I had been using two different timers based on a PLL to feed two different GPIO pins. It may be creating some timing shifts that my hardware (custom ASICs) don't like. I tried feeding both GPIO from the SAME Timer, and I only seem to get an output on one. Is this to be expected?

Thanks!
3 REPLIES 3
Posted on September 19, 2014 at 16:36

What?

Posted on September 19, 2014 at 16:53

Well each timer only has a single counting element, if that's what you mean.

I think you need to describe or diagram the nature of the connections and signals.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
jvavra
Associate III
Posted on September 19, 2014 at 17:04

Guys,

Nevermind, turns out the answer can be found in the datasheet (of all places!). Thanks anyway for the replies.