cancel
Showing results for 
Search instead for 
Did you mean: 

Cascaded Timer Causes Delay

jvavra
Associate III
Posted on October 03, 2014 at 16:14

Using the STM32427, with TIM5 set up as a master to TIM1 and TIM8. This works fine; I get synchronous pulses like I expect. However, I'd also like to have TIM1 act as master for TIM4. When I enable TIM1 in master mode, it suddenly is no longer synchronous w/ TIM5/TIM8.  

#stm32-timer
1 REPLY 1
chen
Associate II
Posted on October 03, 2014 at 16:43

Hi

I thought I had answered you before.....

''When I enable TIM1 in master mode, it suddenly is no longer synchronous w/ TIM5/TIM8.  ''

I am not sure what happens if you cascade timers as masters ie

TIM5 is master to TIM1 and TIM8

TIM1 is master to TIM4

Why do you not make TIM4 a slave to TIM5 as well (if that is possible - I am not sure)?