2017-09-25 01:10 PM
I just installed STM32CubeMX on my Windows 10 machine. When I try and launch it, I get the following error. How can I fix this? I have Java installed- for many environments and the Java About returns the message below
2017-09-25 01:19 PM
>> How can I fix this?
Go into the registry and find the node that points to a deleted/replaced version of Java. Then delete that node.
2017-09-25 04:11 PM
I tried that but I still get the same message. Any chance you could tell
me which registry entry it is looking at?
On Mon, Sep 25, 2017 at 4:20 PM, Clive One <st-microelectronics@jiveon.com>
2017-09-25 05:10 PM
I'm sure it is enumerating through them, so machine specific.
I've seen JRE updates do a clean-up. Might want to double check for 'Installed Programs', making sure there aren't assorted versions.
https://www.java.com/en/download/faq/remove_olderversions.xml
ST might be able to provide specifics of what they enumerate, or be able to provide additional diagnostic output, I am not ST.
Check also if anything is listed in the PATH environment variable. Open a DOS Box, type PATH