cancel
Showing results for 
Search instead for 
Did you mean: 

H3LIS332DL Interrupt events

hmai
Associate
Posted on October 23, 2013 at 11:48

As Interrupt sources, what means the ''X/Y/Z High Event'' or ''... LOW Event'' in the datasheet?

Are there defined trigger values for these events, and are they changeable in some registers?

#h3lis331dl #accelerometer #application
1 REPLY 1
Thiago REIS
Associate II
Posted on November 18, 2013 at 13:39

Hello Mai,

This section of the interrupts means that the interrupt will occurr either when the acceleration value is higher or lower than the determined threshold value.

Please check on page 30 of the attached datasheet for the configuaration of the interrupt registers and on page 32 for the thresholds setup.

Please let me know if this helps with your question,

Thank you,

Thiago

________________

Attachments :

H3LIS331DL.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzLP&d=%2Fa%2F0X0000000bKH%2FV46QYBE_NCTUfl2Bg7EaHWgS1H8cvyQQatVt8QokIro&asPdf=false