2013-12-03 08:22 PM
Hello ,
I have configured systick for 1 ms in Discovery Board using Systick_config function.But I am not getting properly 1 ms...SystemCoreClock = 144 MHz...
Urgent Help needed ...... #stm32-systick2013-12-04 08:50 AM
Help needed ...... The math is simple, perhaps it is the clock settings that are wrong? Check your PLL settings/sources in system_stm32f4xx.c, and output clocks via MCOx or TIM pins to confirm the core is actually running at the speed you want. Or avoid hard coded values? uint32_t SystemCoreClock = ((HSE_VALUE / PLL_M) * PLL_N) / PLL_P;