cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 L1 Discovery - Failed to read CPUID for Cortex device

ecatala
Associate II
Posted on June 12, 2014 at 14:12

Hi,

I am using the IDE from EWARM IAR Embedded Workbench for ARM 6.40.2

and a ST-LINK to download the demo project to the evaluation board STM32L152RCT6 and I get the error Failed to read CPUID for Cortex device

 

 

Best regards,

Estanislao
1 REPLY 1
Posted on June 12, 2014 at 15:43

Perhaps it is entering a low power mode and losing debug connectivity? You could reset with BOOT0 pulled/set high, this would get you into the System Loader and permit recovery of the board.

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..