cancel
Showing results for 
Search instead for 
Did you mean: 

Does the APWorkbench tool supports any scripting language?

nmagniez
Associate II
Posted on November 11, 2013 at 13:51

Does the APWorkbench tool supports any scripting language?

1 REPLY 1
Marco VENERI
Associate II
Posted on November 12, 2013 at 15:28

Yes, the tool supports a scripting language enabling operations such as I2C register read/write, IIR coefficient read/write, simple loops, pauses, dumping of the relevant information and monitoring of specific bits of supported devices.

Scripting commands can be loaded from a file on disk, refer to the ''Run script...'' item in the ''File'' menu. A convenient shell interface is also included in order to issue commands - through the ''Log View'' button. Typing ''help'' will list the available commands.

Note: the tool can also be used as a generic I2C I/O interface - with logging capabilities - by selecting the ''APWLink Audio Interface'' in the Launch Wizard startup dialog.

http://www.st.com/web/en/catalog/tools/PF253187

required.