cancel
Showing results for 
Search instead for 
Did you mean: 

During the APWorkbench setup process FTDI drivers are optionally installed. Can you explain what it is for and if I should install it?

nmagniez
Associate II
Posted on November 11, 2013 at 13:50

During the APWorkbench setup process FTDI drivers are optionally installed. Can you explain what it is for and if I should install it?

1 REPLY 1
Marco VENERI
Associate II
Posted on November 12, 2013 at 15:13

FTDI drivers are used by APWorkbench suite to communicate with the hardware

http://www.st.com/web/en/catalog/tools/FM116/SC1028/PF253187

, via USB.

Driver installation is required in case evaluation boards using APWLink have to be operated (typically all 

http://www.st.com/soundterminal

amplifier boards). FTDI drivers are not required for MEMS Microphone evaluation kit since it makes use of a different USB interface,

http://www.st.com/web/en/catalog/tools/FM116/SC1028/PF258331

.

Updated drivers can be downloaded from FTDI website (D2XX version):

http://www.ftdichip.com/Drivers/D2XX.htm

Note: admin rights are required to install FTDI drivers.