cancel
Showing results for 
Search instead for 
Did you mean: 

Could your recommend a class D amplifer,the supply voltage is 12Vdc,mono BTL,output 50W~100W.Thanks!

nmagniez
Associate II
Posted on February 04, 2014 at 16:59

Could your recommend a class D amplifer,the supply voltage is 12Vdc,mono BTL,output 50W~100W.Thanks!

1 REPLY 1
Nickname1623_O
Associate II
Posted on February 10, 2014 at 03:29

hi naue_b ,since the output power had been limited by supply votlage , even the load impedance is 2 ohm , the max 10% THD output power is around 35W, it's far away from your target output power . but if the supply votlage was 20V, TDA7498E can meet your reqirement.

Thanks