cancel
Showing results for 
Search instead for 
Did you mean: 

Music and notification MP3 player

nmagniez
Associate II
Posted on February 27, 2014 at 11:32

For our industrial application, we implemented a STA013 to play sound files located on a SD card. We have to play background music and sometimes play some notification sound. So we send background music MP3 to STA013 and when we have to play a notification sound, we stop the music flow, to send to STA013 the notification MP3, and restart flow of the background music. This method works correctly, but we have some trouble on the change of MP3 flow : a glitch is often heard when the MP3 flow change. We assume its comes from the brutal change of flow. We search a solution, like void mp3 buffer of sta013, or a soft reset.

To avoid to many calibration of sta013, every mp3 have been reencoded to have the same characteristics.

Have you already met the problem ? Have you some idea to destroy this glitch ?

1 REPLY 1
Nickname1623_O
Associate II
Posted on March 03, 2014 at 03:35

Hi Naue_b ,

noramlly the source switching would introduce some pop or click noise , to avoid this kind of noise , you may mute the amplifier output when you going to switch input source to block pop noise before speaker , then  audible noise will  not be presented .

another way is using a mixer to adjust background music volume and increased notification voice level , this kind of feature will be available in audio processor IC.

Thanks