cancel
Showing results for 
Search instead for 
Did you mean: 

What is the clock frequency where the mics switch from normal mode to sleep mode?

nmagniez
Associate II
Posted on February 04, 2014 at 16:57

What is the clock frequency where the mics switch from normal mode to sleep mode?

2 REPLIES 2
Alessandro MORCELLI
Associate II
Posted on February 07, 2014 at 11:27

Actually the threshold of the switch between normal mode and sleep mode is not fixed. There is an hysteresis. In fact the microphone changes its behavior when the clock frequency is comprised between 500kHz and 700kHz

Regards,

Alessandro

Alessandro MORCELLI
Associate II
Posted on February 07, 2014 at 11:30

Addition to previous statement.

Basically the microphones switches off when the clock frquency decreases to value lower than 500kHz but switches on for frequencies over 700kHz.

Alessandro