cancel
Showing results for 
Search instead for 
Did you mean: 

why MicroXplorer don't know the STM32F051 in LQFP32..??

ffred
Associate II
Posted on January 25, 2014 at 14:15

Hi all,

why the LQFP32 versions of STM32F051 are not available in MicroXplorer ..???

(STM32F051KxTx)

Thanks

Fred

#stm32cube #stm32cubemx
1 REPLY 1
Amel NASRI
ST Employee
Posted on February 20, 2014 at 16:55

Hi Fred,

I am pleased to inform you that this product is supported in STM32CubeMX.

The STM32CubeMX is part of STMicroelectronics STM32Cube™.

STM32Cube™ is an STMicroelectronics original initiative to ease developers’ life by reducing development efforts, time and cost. STM32Cube™ covers STM32 portfolio.

STM32CubeMX graphical configuration tool simplifies and automates configuration and generation of STM32 initialization C code ready to be used with several development environments. The tool provides:

- an easy-to-use filter for selecting the desired STM32 device and graphical wizards to simplify configuration

- the pin-out wizard assists pin assignment to avoid conflicts, embedding a powerful constraints solver

- the clock-tree wizard assigns clocks and performs dynamic validation

- the peripherals-and-middleware wizard aids configuration to avoid unusable settings

- the power-consumption wizard checks that the application meets the available power budget.

The STM32CubeMX tool and STM32CubeF4 embedded software are available immediately, free of charge, directly from

http://www.st.com/stm32cube

.

Best Regards,

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.