cancel
Showing results for 
Search instead for 
Did you mean: 

stand alone SWIM programmer/sample code?

tim
Associate
Posted on November 17, 2013 at 22:48

I suddenly find that we need a couple of stand alone programmers for our STM8L052 board. By ''stand alone'' I mean the application code will have to be loaded into the programmer and it will flash the production units via SWIM. The operation will just plug it in and press the button; no connection to a PC allowed.

Anybody know of such a thing?
1 REPLY 1
jdf25252
Associate II
Posted on November 21, 2013 at 20:12

Look at the Segger ''Flasher STM8'' or the P&E ''Cyclone ST''.  I've used both though NOT for STM8.  The Cyclone is REAL nice (I use one for Freescale ''HCS08'' but pricey.  I'd check the Flasher carefully.  I'm not exactly sure it'll operate stand alone.

jdf