cancel
Showing results for 
Search instead for 
Did you mean: 

Latest download of STVD very slow saving files

ted
Associate
Posted on November 22, 2013 at 01:12

I downloaded the latest STVD using the Cosmic compiler and set up a new project.  When I edit a file and then try to compile it, it takes about 30 seconds to a minute to save the file before doing the compile.  Makes using it almost not worth it.  Any ideas on what setting could be wrong?

#stvd---cosmic-configuration
1 REPLY 1
S C
ST Employee
Posted on November 22, 2013 at 10:42

Hello,

The delay might come from a wrong Cosmic licence handshake when launching the build. Is the build successful at the end ? Is the file saving done directly through the STVD menu (or Ctrl+S) or is the file saving automatically managed by STVD after a ''Build'' (F7) action from user ? Saving the file directly through STVD menu will show if the delay comes from the file saving action itself rather than from the ''Build'' initialization.