cancel
Showing results for 
Search instead for 
Did you mean: 

Problems found in STM32F746G-discovery Kit schematics

NEERAJ GUPTA
Associate II
Posted on July 19, 2017 at 14:11

Refering to page no 6 in  mb1191.pdf  which is available as STM32F746G-discovery Kit schematic. 

The pin diagram of following two Arduino connector was incorrect, this need correction as follows:

1. CN4 connector has ARD_D5 pin mentioned as PA8 -> this is incorrect.

    ARD_D5 pin should be connected with PI0 as per rest of schematic.

2. CN7 connector has ARD_D10 pin mentioned as PI0 -> this is incorrect.

    ARD_D10 pin should be connected with PA8 as per rest of schematic.

Please! do this correction urgently. Otherwise it will create a lot of confusion regarding the hardware design.

3 REPLIES 3
Imen.D
ST Employee
Posted on July 19, 2017 at 16:54

Hello

GUPTA.NEERAJ

,

Thank you for bringing this issue to our attention.

You are right,

I will highlight this typo error to correct it in coming releaseofSTM32F746G-DISCO schematics pack.

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on July 19, 2017 at 19:02

Reported two years ago...

https://community.st.com/0D50X00009XkgDCSAZ

 

https://community.st.com/0D70X000006SoTcSAK

 

https://community.st.com/0D50X00009XkZ5xSAF

 
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on July 20, 2017 at 06:52

Thanks for acknowledging this.