2014-03-29 11:13 AM
Dear All,
I would like to upgrade / update the STM32F429 firmware using a USB Key.I have found one application note, but I have not found any working example.Does anyone have some working example or some advise?Let me know!Best regards2014-03-29 11:21 AM
2014-03-31 08:02 AM
Dear Clive1,
thank you very much for the answer and the advise.Is it possible to use the same code also on the STM32F429 EVAL board changing theSTM32F429I_Discovery file with the EVAL's one?Let me know!Best regards2014-03-31 08:27 AM
The examples are reasonably portable. You have to pay attention to pin utilization, and differences in crystals (8 MHz vs 25 MHz, and associated PLL settings, and HSE_VALUE)
2015-03-11 04:44 AM
Dear Sir,
I am using this program to update my device, after I update the device, it can not automaticly boot after power off. I have to push the reset button each time when I power it on .2015-03-11 06:22 AM
I am using this program to update my device, after I update the device, it can not automatically boot after power off. I have to push the reset button each time when I power it on.
You'll probably want to instrument the code so you can identify where and how is locking up, or malfunctioning.