cancel
Showing results for 
Search instead for 
Did you mean: 

LIS3DSH - error offset

tdecamps
Associate
Posted on December 12, 2013 at 18:48

hi,

I use LIS3DSH and a problem appear sometime at init, in fact we catch false value from chip (offset error on x axis).

Only offset is not correct (same offset value in case of pb).

SPI bus reading is correct , value come from chip.

Do you have any reason for that , may we use any control to indentify error ?

Thnaks in advance,

Regard,

1 REPLY 1
Thiago REIS
Associate II
Posted on January 10, 2014 at 14:09

Hello Thierry,

What is the value that you are reading for the initial offset value?

If possible, could you please attach the section where you setup CTRL_REG2 (21h) and an image showing the measured values?

Thank you,

Thiago Reis