cancel
Showing results for 
Search instead for 
Did you mean: 

STM MCU with embedded 485

ionutF
Associate III
Posted on February 17, 2016 at 15:48

Is there a STM MCU with RS-485 integrated on it ? It would be very usefull  given the fact that MCUs are industriall devices and one of the most used communication protocol in industry is RS-485.   

2 REPLIES 2
Nesrine M_O
Lead II
Posted on February 17, 2016 at 16:58

Hi ionut.fasola,

RS485 Driver Enable is a hardware feature implemented in USART for 

F0/F3/F7/L4/L0 products.

-Syrine-

Posted on February 17, 2016 at 18:28

Having the driver circuitry on chip isn't really appropriate for a general purpose micro-controller. If you want CAN, RS232 or RS485 you need to integrate the appropriate off-the-shelf driver chips into your design.

The drivers likely use wholly different processes and geometries.

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..