cancel
Showing results for 
Search instead for 
Did you mean: 

RM0351 RTC wakeup

turboscrew
Senior III
Posted on September 10, 2017 at 16:20

In the STM32L4x5/4x6 reference manual (and some other manuals too, like RM0090) the figure 374 shows that the RTC wakeup timer can be clocked with ck_apre, but the description of RTC_CR says that the alternate input is ck_spre.

Can someone confirm that the register description is right and the picture is wrong?

1 REPLY 1
Imen.D
ST Employee
Posted on September 11, 2017 at 17:02

Hello

Aaltonen.Juha

,

I confirm the typo in the RTC block diagram picture.

RTC_WUTR must receive 2 inputs :

  • One from WUCKSEL prescaler output
  • One from ck_spre (RTC_PRER synchronous prescaler output) and not from ck_apre which is a mistake in the block diagram.

This is a known error reported internallyand will be fixed in coming releases of the reference manual (as for other series of manuals too).

Thanks

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen