cancel
Showing results for 
Search instead for 
Did you mean: 

Transfer variable contents from STM32F4 to MATLAB

kriscicluna
Associate II
Posted on December 28, 2013 at 14:27

I would like to know if there exists a sample code on which I can elaborate to do the following:

Transfer data stored in a variable on the microcontroller to computer software such as MATLAB through the USB OTG interface. 

1 REPLY 1
Andrew Neil
Evangelist
Posted on December 28, 2013 at 18:48

Pretty sure MATLAB can use a COM port - which would include a Virtual COM port...

Check MATLAB documentation to see what it supports...