cancel
Showing results for 
Search instead for 
Did you mean: 

Help me choose a programmer [newbie]

chris2399
Associate
Posted on January 08, 2014 at 21:05

I have a legacy system that uses a STM32F103RE device and I would like to connect to it via JTAG (or any other on board option) and view the code on the device to verify it's version (and possibly update).  It seems like the Rlink Standard programmer and free software will do the trick.

What are your expert thoughts?
4 REPLIES 4
Posted on January 08, 2014 at 21:20

What are your expert thoughts?

ST-Link, it's cheap and has inspection utilities/tools. Works only with ST parts, or subset thereof.

J-Link, it's professional, and is a commercial product that Segger supports and updates regularly. It works on a vast array of parts.

U-Link, perfectly adequate, works on many parts, only works with Keil tools
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
chris2399
Associate
Posted on January 08, 2014 at 22:02

The J-Link looks very capable and could likely be useful in other applications.

Thanks for your help.

chen
Associate II
Posted on January 09, 2014 at 11:51

Hi

If this is for personal use, Seger do an 'Educational' version of j-Link which is very cheap.

It can only be used for non- commercial use!

dmg0048
Associate II
Posted on January 09, 2014 at 21:01

I think the cheapest alternative would be ST-Link  and EmBlocks.